Points Used on Advanced OPC Groups

Advanced OPC Points read and/or write to items on OPC DA servers. You need to map the items on each OPC DA server to suitable Advanced OPC Points within the ClearSCADA database. This enables ClearSCADA to perform the relevant processing handle the data in a similar way to other point data on the system (for instance, monitor state changes, raise alarms, or execute controls).

The Advanced OPC Driver supports the point types that are listed below. You configure the points using the properties on the relevant Advanced OPC Point Form.

For information on creating a point and displaying a Point Form, see Configuring a Point.

For information on configuring fields on the <Advanced OPC Point Type> tab on the Point Form, see the references below:

The Advanced OPC Driver supports the controlling of points. Advanced OPC points include a Control tab, which allows you to enable and configure how points are controlled.

The properties on other tabs are common to points on multiple drivers, see Tabs on Point Forms.


Disclaimer

ClearSCADA 2017 R3