Configuring a DDE Server

For every server with which you want ClearSCADA to communicate using the DDE protocol, you need to configure a DDE Server in the ClearSCADA database. In order to configure each DDE Server successfully, you need to ascertain the required settings for that Server (see Preparation). You can then use the fields on the DDE Server Form to configure the DDE server in the ClearSCADA database.

The Form has several tabs.

Use the fields on the DDE tab to:

For information on the fields on other tabs, see Tabs That are Common to Many Configuration Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R3