Configuring Digital Points

Add and configure an ODBC Digital point for each item of digital-type data that you want to transfer between a ClearSCADA system and another application, using ODBC data transfer standards.

Configure the properties of each digital point using the fields on the ODBC Digital Point Form. The Form has several tabs.

Use the fields on the ODBC tab to:

Use the fields on the Query tab to:

For information on the fields on the Digital Point tab, see Defining Digital Point Details in the ClearSCADA Guide to Core Point Configuration.

For fields on other tabs on the Form, see Tabs on Point Forms in the ClearSCADA Guide to Simple Drivers.


Disclaimer

ClearSCADA 2017 R3