SCADAPack x70

Imported Manifest

Associated with: SCADAPack x70 Device Configuration items

You can use the Import from RemoteConnect pick action to import manifest configuration files into ClearSCADA from SCADAPack RemoteConnect software.

The Imported Manifest status attribute indicates the filename and version of the last manifest configuration file to be imported into ClearSCADA for the selected SCADAPack x70 Device Configuration item. The version number increments by 1 whenever you import a newer version of the file into ClearSCADA for that particular Device Configuration item.

 

"unityTRSSDtmManifest", Version 1

For further information about the imported manifest configuration file, use the Imported Manifest status attribute in conjunction with the Device Configuration item's Manifest File n status attribute(s).

If a manifest configuration file has never been imported into ClearSCADA for that particular Device Configuration item, the Imported Manifest status attribute displays the value 'None'.


Disclaimer

ClearSCADA 2017 R3