SCADAPack x70

Manifest File n

Associated with: SCADAPack x70 Device Configuration items

You can use the Import from RemoteConnect pick action to import manifest configuration files into ClearSCADA from SCADAPack RemoteConnect software.

The Manifest File n status attributes indicate the files that are included in the last manifest configuration file to be imported into ClearSCADA for the selected SCADAPack x70 Device Configuration item. There is one Manifest File status attribute per separate file in the manifest. Each Manifest File status attribute is assigned a different number.

 

Manifest File 1 "configuration.rtu"

Manifest File 2 "station.apx"

Manifest File 3 "logicapp1.sta"

Manifest File 4 "logicapp1.sig"


The Manifest File n status attributes for an imported manifest configuration file that contains the 4 files that are listed in double quotation marks above.

For further information about the imported manifest configuration file, use the Manifest File n status attribute(s) in conjunction with the Device Configuration item's Imported Manifest status attribute.

Manifest File n status attributes are only displayed if a manifest configuration file has been imported into ClearSCADA for the selected SCADAPack x70 Device Configuration item.

Further Information

For information about the types of file that might be included in a manifest configuration file, see the documentation provided with the SCADAPack RemoteConnect software.


Disclaimer

ClearSCADA 2017 R3