Configure Wonderware Historian Tag Properties from ClearSCADA

Each Wonderware Historian tag has a set of properties. You can configure these properties from ClearSCADA by creating custom metadata fields which are mapped onto the tag properties. For some properties, ClearSCADA will automatically configure the property with a default value. For example, ClearSCADA will configure the EngineeringUnit property with the Units for analogue and counter points. However, you can override this default by defining a custom metadata field for the property.

You cannot configure some properties. Their values are fixed by ClearSCADA or HCAL.

When ClearSCADA creates a tag in Wonderware Historian, it automatically configures the tag’s properties. It uses the metadata field values of the point or accumulator. If you change a metadata field value that is mapped onto a tag property after a user has created the tag, then ClearSCADA will either update the tag:

To create a metadata field in ClearSCADA, use the Metadata Window to Add or Modify an Extra Field.

When ClearSCADA prompts you to select the type of field that you want to add, select Standard.

The Edit Field window is displayed.

Enter the following:

For details about the other fields in the window, see Add or Modify an Extra Field in the ClearSCADA Guide to Server Administration.

You can map a ClearSCADA metadata field to each of the Wonderware predefined tag properties listed below. Follow the links for more details about these properties, including theType that you need to enter in the Edit Data Field window when you create the metadata field. The information also includes the default value of each Wonderware Historian predefined tag property. ClearSCADA will overwrite this default value if you create a metadata field for the tag property.

The following are Wonderware Historian predefined tag properties that have fixed values. If you create a ClearSCADA metadata field for any of these properties, ClearSCADA will log an error and will not use the metadata field.

The following are the Wonderware Historian predefined tag properties that either do not apply or are not useful in ClearSCADA. If you create and configure a ClearSCADA metadata field for any of these Wonderware tag properties, the tag property will retain its value regardless.

Further Information

Wonderware Historian Tags


Disclaimer

ClearSCADA 2017 R3