Unacknowledge an Alarm

The ability to Unacknowledge Alarms is disabled on most systems by default. (Its permission is typically denied on a per server basis.)

Depending on the system configuration, it may be possible to unacknowledge alarm(s) that have been acknowledged, but for which the abnormal condition still exists (that is, alarms that are in the Acknowledged Uncleared state). You unacknowledge alarms using the Unacknowledge or Unacknowledge Alarms options. (A further option, Unacknowledge with Comment can also be used—see Unacknowledge an Alarm with Comment.)

When you unacknowledge an alarm:

NOTE: In addition to the pick actions mentioned here, Geo SCADA Expert provides various methods that enable activities to be performed on alarms programmatically. This includes methods that are designed to trigger activities at specific times, such as the AcceptAtTime method that can be used to specify the time at which Geo SCADA Expert is to acknowledge an alarm and to optionally log a comment for that acknowledgment. For more information on such methods, see the Database Schema (specifically the Methods section in the CAlarm class).


Disclaimer

Geo SCADA Expert 2019