Launch a Window Container in Full Screen Mode

You can use a Startup Configuration File to display a Window Container in full screen mode when the ViewX client launches.

When a Window Container launches in full screen mode, the following occurs:

To launch a Window Container in full screen mode, use the DisplayMode attribute in the Startup Configuration File. For further information about this attribute, see XML Elements.

Example:

The example below shows a Mimic displayed in a Primary Window Container in Full Screen mode.

This example uses the following XML code within the WindowContainer tags in the Startup Configuration File.

<PrimaryWindowContainer MonitorOrigin="0,0" DisplayMode="FullScreen"/>

Observe that the DisplayMode element for the Primary Window Container is set to "FullScreen".

If the current user has Can Toggle Full Screen enabled in their User settings (see Define the General Settings for a User in ViewX), they can turn off full screen mode. To do this:

Or:

If the DisplayMode attribute is set to "FullScreen" for any of the Window Containers defined in the Startup Configuration File, this will override the Start Full Screen setting on the ViewX Options window (see Miscellaneous Options for ViewX Clients). If this is the case, the Options window will display the following:

NOTICE

unexpected behavior OF APPLICATION

Startup Configuration files are intended only for use on ViewX clients that are required to launch Geo SCADA Expert on a Multi-Monitor setup, and/or have customized Window Container behavior.
Do not use Startup Configuration files on Virtual ViewX clients, as these clients only support a single monitor setup, and do not support the same customized behavior. Using a Startup Configuration file on such a client could result in unexpected behavior. (Startup Configuration files are not supported, and are ignored, on Original WebX clients.)
Failure to follow these instructions can result in inoperable equipment.

Disclaimer

Geo SCADA Expert 2019