XML Elements

A Startup Configuration File is an XML file. It must contain a valid combination of the elements that are described in this topic.

XML is case-sensitive. To be valid in XML files, Boolean 'true' and 'false' values must be fully lower case.

NOTICE

unexpected behavior OF APPLICATION

Startup Configuration files are intended only for use on ViewX clients that are required to launch Geo SCADA Expert on a Multi-Monitor setup, and/or have customized Window Container behavior.
Do not use Startup Configuration files on Virtual ViewX clients, as these clients only support a single monitor setup, and do not support the same customized behavior. Using a Startup Configuration file on such a client could result in unexpected behavior. (Startup Configuration files are not supported, and are ignored, on Original WebX clients.)
Failure to follow these instructions can result in inoperable equipment.

Further Information

Examples that demonstrate the use of specific XML attributes: see Startup Configuration File, and see Example Configuration.

Troubleshooting - Startup Configuration Files.

Resolve an Invalid Startup Configuration File.


Disclaimer

Geo SCADA Expert 2019