Configure the Execution Settings for a Calculation Point

Use the fields within the Execution section of the Calculation tab to specify the specific triggers that will cause Geo SCADA Expert to execute the calculation expression.

If you set a periodic trigger condition, you can view the next scheduled execution time in the point's status window. For more information, see Calculation Point Specific Status Attributes.

Examples for the Periodic trigger condition:

Example 1:

Interval: 1H, Offset: H+30M, Time Zone: Coordinated Universal Time (UTC).

Geo SCADA Expert will execute the calculation expression every hour, at half past the hour UTC.

Example 2:

Interval: 1D, Offset: D+6H, Time Zone: Local Time with Daylight Saving Time.

Geo SCADA Expert will execute the calculation expression daily at 6am local time, adjusted for Daylight Saving Time.

Further Information

Execute pick action: see Using Calculation Point Specific Actions.

Tags:see Tags in the Geo SCADA Expert Guide to Expressions.

Hand Control: see Hand Control in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.

Internal Points: see Internal Points.

Override: see Override in the Geo SCADA Expert Guide to Drivers.

Release Override:see Release Override in the Geo SCADA Expert Guide to Drivers.

Accumulators: see Configuring Master Station Accumulators in the Geo SCADA Expert Guide to Core Configuration.

Variables: see Using Variables to Store Data Values in the Geo SCADA Expert Guide to Core Configuration.

Random Generators: see Understanding the Random Generator in the Geo SCADA Expert Guide to the Random Generator.

Coordinated Universal Time: see Coordinated Universal Time in the Geo SCADA Expert Guide to Core Configuration.

Daylight Saving Time: see Daylight Saving Time in the Geo SCADA Expert Guide to Core Configuration.


Disclaimer

Geo SCADA Expert 2019