Disable Historic Data Compression

You might decide not apply historic data compression to a point:

Typically, you do not apply compression if the historic updates for the point are not excessive and:

Or:

(Apply Historic Data Compression Settings if a point’s historic values are only used to provide an overview of the data; you want to reduce storage requirements for historic data; or excessive historic updates are effecting system performance.)

To disable the compression feature for a point:

  1. Display the Point Form for the point that you want to configure (see Display a Form in the Geo SCADA Expert Guide to Core Configuration).
  2. Select the Historic tab.

    The Historic tab is only included on the relevant configuration Forms when the Historic Data feature is enabled on the server. The feature enables Geo SCADA Expert to store data historically (see Historic Data Storage Settings).

  3. Set the Apply To field in the Compression section of the Point Form to ‘No Data’.


    The Significant Change and Minimum Interval features are unavailable.
  4. Save the configuration.

Disclaimer

Geo SCADA Expert 2019