Actions Associated with Scanners on Simple Drivers
            The scanners on simple drivers support a combination of these actions:
- Acknowledge Alarms
 - Acknowledge with Comment
 - Alarm Response
 - Cancel Refresh
 - Disable Alarms
 - Disable Scanner
 - Display Points
 - Enable Alarms
 - Enable Scanner
 - Refresh
 - Release Exclusive Control—(Systems on which Exclusive Control is enabled)
 - Remove Alarms
 - Remove with Comment
 - Reset Point Statistics
 - Take Complete Exclusive Control—(Systems on which Exclusive Control is enabled)
 - Take Partial Exclusive Control—(Systems on which Exclusive Control is enabled)
 - Unacknowledge Alarms
 - Unacknowledge with Comment.
 
                            
Further Information
‘Core’ pick actions that are common to many database items: see Object Menu Options in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.
For information on any scanner-specific actions that are not listed above, see the relevant driver guide.