Status Attributes Associated with Slave Sources on Simple Drivers
The sources on simple Slave drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New Slave sources only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only Slave sources that are under Exclusive Control)
- Alarm State
- Alarm Last Updated
- State Alarm
- Alarm Count
- Source Name
- Source
- State
- Comms Statistics.
For information on source status attributes that are not listed above, see the driver-specific documentation.