Configuring a SCADAPack Controller

In addition to the controllers listed below, Geo SCADA Expert can communicate with Realflo-enabled SCADAPack controllers using the SCADAPack Modbus Realflo Extension Driver. For information on Realflo controller types, see the Geo SCADA Expert Guide to the SCADAPack Modbus Realflo Driver.

For each SCADAPack controller that exists on your system, you need to create and configure a corresponding outstation database entry within the Geo SCADA Expert database. When configuring the database, ensure that you select the type(s) of controller and communications that correspond to your system hardware.

The types of controller that the SCADAPack Modbus driver supports are listed below. For further information on the type(s) of controller that best represent your system set-up, see Outstation Types and Communications Set-ups in the Geo SCADA Expert Guide to Advanced Drivers.

The SCADAPack Modbus driver supports these types of controller (outstation):

If your database structure is ‘modular’ and Group Template are used to store ‘model’ SCADAPack Modbus configuration, in addition to the above types of controller, you can add driver-specific ‘abstract’ controller items to your Group Templates:

You can only add Abstract Items to Group Template. The abstract items appear as additional driver-specific entries when you display the context sensitive menu from a Group Template. As with other abstract items, in order to represent a ‘real’ controller, you need to convert the abstract items into the required type of controller (outstation) within the Group Instance that reference the Group Template. For more information, see Add an Abstract Item to a Group Template in the Geo SCADA Expert Guide to Core Configuration.

For each SCADAPack controller that exists on your system, you need to specify the controller features using the fields on the appropriate SCADAPack Outstation Form. (Unless the SCADAPack controller has additional features enabled that are supported by a SCADAPack Modbus Extension Driver—in which case, see the relevant section in the appropriate SCADAPack Modbus extension driver guide.)

Each SCADAPack Outstation Form has several tabs.

Use the fields on the SCADAPack tab to:

With Direct and Shared Outstations, use the Direct tab to:

Use the PSTN tab to define the Public Switched Telephone Network properties for a controller (see Define an Outstation’s PSTN Properties in the Geo SCADA Expert Guide to Advanced Drivers.)

Use the Network tab to define additional properties for any network connected controller (see Define an Outstation’s Network Properties in the Geo SCADA Expert Guide to Advanced Drivers). (Port number 502 is the Modbus TCP port that is registered for use with the IANA (Internet Assigned Numbers Authority).)

Use the Shared tab to:

The fields on other tabs are common to controllers and outstations on many advanced drivers (see Tabs on Outstation Forms in the Geo SCADA Expert Guide to Advanced Drivers).

For information on the minimal amount of configuration that you can undertake to produce a functional SCADAPack controller in Geo SCADA Expert, see Minimum Configuration.

If your Geo SCADA Expert system is running the SCADAPack Modbus Realflo Extension Driver, to communicate with SCADAPack controllers that have Realflo enabled, see the relevant configuration section in the Geo SCADA Expert Guide to the SCADAPack Modbus Realflo Driver. The configuration Forms for such controllers contain a Realflo tab in addition to the SCADAPack tab covered in this section.


Disclaimer

Geo SCADA Expert 2019