SQL Technical Reference

This section provides a technical reference for the SQL features supported in Geo SCADA Expert.

Information about the conventions used in this section are described in the Notation topic. Information about the Data Types supported in SQL commands can be found in the Data Types page

The SCADA server supports four types of SQL command:

Contents

Name Description
CaseExpression Functions selecting a value conditionally
Conditions Syntax of conditions that can appear in a WHERE or HAVING clause.
DistanceFunctions A function returning distance values.
Expressions Syntax of scalar expressions.
NumericFunctions A function returning a numeric value
StringFunctions A function returning a string value

Disclaimer

Geo SCADA Expert 2019