Read Permission Browse Permission Control Permission Override/Release Permission Acknowledge Alarms View Alarms Permission Remove Alarms Permission Manual Redirection Permission Unacknowledge Alarms Assign Responsibility Permission Edit Notes Permission Retrieve Data Promote Permission Tune Limits Annotate History Modify History Permission Validate History Disable Points Disable Alarms Disable Controls Permission On/Off Scan Switch Line Permission Diagnostics Permission Cancel Request Exclusive Control Permission Manage Excl. Ctrl Configure Permission Security Permission System Admin Permission

Permissions for Database Items

Each user account and User Group has permissions that define which features can be accessed when a user logs on. The permissions are applied to each database item separately, for example, a user may have access to controls on one point but not on another.

The permissions for each item are set via the item's Security window. You can use the Security window to define which user accounts have access to the item, and which features are available to those accounts.

The permissions shown in the Security window vary, according to whether any permissions have been denied.

In ViewX, the permissions that you allocate to a user account only take effect if that user account has been configured to have the corresponding ViewX features enabled. The ViewX features for each user account are enabled or disabled on the User Form (see Creating a User Account).

When you set the access permissions for a Group, the same permissions may also be inherited by the items within that Group:

Items in Groups can have different permissions to the 'parent' Group, you can alter the permissions of each item in a Group as required.

Access permissions for Group Templates and Group Instances work differently—Group Instances do not inherit the permissions from their Group Template; the permissions for Group Instances are set via the security settings for the Group Instance.

When you change permissions, certain menu options will remain visible to users even if they do not have the permissions to use them. If the users attempt to use such options, an Access Denied message box is displayed. If the users log off and then log on again, those options to which they do not have access will no longer be displayed.

To allocate a permission, select the appropriate check box. If you want to deny a permission, clear its check box. When a permission is selected for a User Group or User Account a Short Code appears alongside the group or account. Certain combinations of permissions are grouped as Operator, Configuration and Advanced.

The security permissions for each database item, associated short codes and default groupings are listed in the following table:

Permissions Short Code Operator Configuration Advanced
Read

View

X X X

Browse

BRS X X X

Control

CTL X X X

Override/Release

OVR X X X

Acknowledge Alarms

ALM X X X

View Alarms

VWA X X X

Remove Alarms

RMA X X X

Manual Redirection

RDR X   X

Unacknowledge Alarms *

UNA     X

Assign Alarm Responsibility *

ARS      

Edit Notes

NOT X X X

Retrieve Data

RET X X X

Promote

PRM X X X

Tune Limits

TUN X X X

Annotate History

AHS X X X

Modify History

MHS   X X

Validate History

VHS   X X

Disable Points

DIS   X X

Disable Alarms

DLM   X X

Disable Controls

DCT   X X

Off/On Scan *

OFS   X X

Switch Line

SWL   X X

Diagnostics

DIA   X X

Cancel Request *

CAN   X X

Exclusive Control

EXC   X X

Manage Excl.Ctrl

MEC   X X

Configure

CFG   X  

Security

SEC      

System Admin

ADM      

* By default these permissions are restricted and not visible in the Security window, see Use Server Side Permission Restrictions.


Disclaimer

Geo SCADA Expert 2019