Configuration Changes Audited Origins

The Auditing Origins settings allow you to choose which types of configuration changes are recorded. Each configuration change has an ‘origin’ which indicates the type of action or interface that caused the change to occur.

You can choose which types of configuration change are recorded on your system. Select the check boxes for those origins that correspond to changes you want to be recorded. Clear the appropriate check boxes for those changes you do not want to be recorded.

The origins are categorized as follows:


Disclaimer

Geo SCADA Expert 2019