Image File

Associated with: WITS Firmware Image.

 

The Field Device's Firmware Image file contains the device's operating system software.

 

The Image File attribute shows the following information for the Firmware Image file:

 

The Image File attribute shows this file information in the following format:

"<filename>" last modified at <time> (<file size> bytes).

 

If there is no file associated with the firmware image, then the Image File attribute shows 'None'.

Further Information

Download Firmware.

Export Image

Import Image


Disclaimer

Geo SCADA Expert 2019