Specify the Direct Properties for a WITS Outstation

If your WITS Field Device uses a direct connection to Geo SCADA Expert, such as a radio connection, you will need to configure the Direct settings. These are shown on the Direct tab of the WITS Outstation Form (for WITS Direct Outstations and WITS Shared Outstations).

Direct settings are only available for WITS Direct Outstations and WITS Shared Outstations.

For information on displaying the Outstation Form, see Display a Form.

WITS Outstation Form - Direct tab

The Direct tab is organized into separate sets of fields:

WITS Field Devices have a limited number of connections, see Connections Limit for WITS Field Devices.


Disclaimer

Geo SCADA Expert 2019