Telephone Number for WITS Dial Up Network Connections

WITS allows for Field Devices to connect to a Master Station via a dial-up network, where the Field Device makes a telephone call to initiate a network connection.

If your network architecture means your Field Device needs to use a telephone call to initiate a network connection to Geo SCADA Expert, you will need to specify the Telephone Number. This is a setting in the Inbound Connections section of the WITS Outstation Form's Network tab.

For each Inbound Connection that uses the dial up network, enter the network connection details. These , include the Telephone Number for connecting to the network containing your Geo SCADA Expert server(s).

Further Information

Display the WITS Outstation Form: see Display a Form.

Host Address and Port: see Define an Outstation's Network Properties

Device Port for WITS Network Connections

TCP/IP Type for WITS Network Communications

End Point for WITS Network Connections


Disclaimer

Geo SCADA Expert 2019