Define the Retry and Timeout Properties for a Pager Service

In normal conditions, the Pager Driver sends a message to a pager or mobile telephone and receives a confirmation message in response (this response may be from the device or from the network provider). This confirmation message allows Geo SCADA Expert to determine whether a message was sent and received successfully.

However, on systems where there are networking problems or interference, the Pager Driver may fail to receive a response to the messages it transmits. When a Pager Driver fails to receive a response, it either:

or

You can use the Pager Service Form to define:

To define the maximum number of retries for a Pager Service:

  1. Display the Pager Service Form.
  2. Select the <Pager> Service tab, for example, for a Multitone Pager Service, select the Multitone Service tab.
  3. In the Retries field, specify the maximum number of times that the Pager Driver will attempt to re-send a message that previously failed. Remember that this setting is for re-sending the entire message and is only used after the Comms Retries of the Pager Channel have attempted.

    The default setting is 2, which is suitable for many systems. However, you can increase or decrease this amount as required.

    We recommend that you limit any increases to the Retries limit so that it is lower than 10. A Retries limit of more than 10 may result in long delays between a message being sent and that message being recognized as failed (if the transmission is unsuccessful).

    With TAP and UCP Pager Services, each retry is sent in a separate call. So if an initial message attempt is unsuccessful, the call will be terminated and a new call will be established for the retry attempt(s).

  4. In the Timeout field, enter the amount of time (in seconds) that has to pass before the Pager Driver attempts to create a new call for a retry attempt. The default amount of 30 seconds is usually appropriate, but you may need to change the setting if the service provider requires an extended period. Your service provider should be able to provide you with information on a suitable timeout setting.
  5. Save the configuration (see Saving Configuration Changes in the Geo SCADA Expert Guide to Core Configuration).

Further Information

Define the Number of Communications Retries for a Pager Channel.


Disclaimer

Geo SCADA Expert 2020