DisplayObjectMenu

The DisplayObjectMenu function allows a script to display the pick action menu for a specified database item.

Syntax

DisplayObjectMenu (Object Reference, Options)

Description

Displays the pick action menu for a specified database item.

Arguments

Object Reference {string}

The address of the database item that has the pick action menu that you want the script to display.

Options {string}

You can choose to exclude some of the menu options from the menu. To do this, add the relevant No option to the syntax, using an ampersand & to separate each option that is to be excluded. Any options that are not excluded are shown in the menu. The No options are:

Returns

None.

Example:

DisplayObjectMenu("CentralGroup.DigPoint1", "NoProperties&NoMethods")

This sets the script to display the pick action menu for the 'DigPoint1' point. The pick action menu shows each of the options for the 'DigPoint1' point except the Edit Properties option and the various method options.


Disclaimer

Geo SCADA Expert 2020