Common Configuration for WITS Database Points
Some WITS-specific configuration settings are common to several types of WITS database point. For example, Persistence settings are available for analog, binary, integrator, and rate-of-change points.
Those settings that are common to multiple types of WITS database points are explained in the following sections:
- Specify a Parent Point
- Persistence for WITS Database Points
- Severity Types and Actions for WITS Database Points
- Profiles for WITS Database Points
- DNP3 Object Flag Actions
- Periodic Logging of Data for WITS Database Points
- Historic Data Filter for WITS Database Points
- Incident Logging for WITS Database Points.
These common settings are applicable to more than one type of WITS database point, but not necessarily all types of WITS database point. For example, alarm limits are not applicable to binary points.