Import Configuration

Associated with: WITS Outstations.

Security permission required to access this pick action: Configure.

NOTICE

INCORRECT CONFIGURATION

Always verify that the configuration you are importing is the correct configuration for the Outstation. If you import incorrect files, the incorrect configuration may replace any correct configuration that is already in place in Geo SCADA Expert. For this reason, take care when selecting the import configuration files and when choosing Merge or Replace.
Failure to follow these instructions can result in incorrect configuration.

You can use the Import Configuration action to import a WITS Field Device's configuration into Geo SCADA Expert. Typically, you will need to use the Import Configuration action as part of your chosen configuration strategy (see WITS Configuration Strategies)

If you are going to import the configuration, and the Outstation or any of its points or profiles are in a Group Instance, you need to be aware of:

  • Property Overrides

    If the necessary Property Overrides are not defined, Geo SCADA Expert will be unable to write the changes to the database and the import process will be unsuccessful. For more details, see Property Overrides.

  • The Point Conversion Process

    As part of the import process, Geo SCADA Expert may need to change the type of existing points in the Geo SCADA Expert database. For example, it may convert an Analog Input into a Minimum point so that it matches the configuration being imported. This conversion cannot take place if the point is in a Group Instance, as its type is determined by the matching point in the Group Template. For more details, see Importing/Uploading Configuration - Point Conversion.

If an import fails as a result of missing Property Overrides or point conversions being required, Geo SCADA Expert lists the configuration errors in a configuration report (see Configuration Reports for WITS Field Devices). There are no changes made to the Geo SCADA Expert database.

When you select the Import Configuration action, the Import Configuration window is displayed. It can contain the following settings:

Import Configuration - WITS Outstation

When you select the OK button, Geo SCADA Expert begins the import process. It updates/replaces the existing configuration for the Field Device's Outstation, Points and Profiles using some or all of the configuration from the imported incremental configuration file.

If the import process is unsuccessful, no changes are made to the configuration and an error report is generated. The report indicates the reasons for the import failure (see Configuration Reports for WITS Field Devices).


Disclaimer

Geo SCADA Expert 2020