Importing and Exporting (WITS)
The WITS driver allows you to import a variety of WITS-related information, including:
- Device Profiles (see Importing a WITS Device Profile XML File)
- Configuration (see Import Configuration)
- Application programs (see Import Program)
- Firmware update files (see Import Image).
You can also use Geo SCADA Expert to create export files that can be used in external applications, such as vendor-supplied Configuration Applications:
- Device Profiles (see Exporting a WITS Device Profile XML File)
- Configuration (see Export Configuration)
- Application programs (see Export Program)
- Firmware update files (see Export Image).
Further Information