Making Changes to WITS Field Device Configuration
            If you need to make changes to the configuration of a WITS Field Device (that has already been set up to work with Geo SCADA Expert), you have three options:
- 
                    
Use Geo SCADA Expert and/or a vendor-supplied Configuration Application to make the changes, and then use Geo SCADA Expert to download the configuration to the Field Device (see Using Geo SCADA Expert to Change Field Device Configuration). You can use Geo SCADA Expert to make changes to the incremental configuration, but changes to the bulk configuration can only be made using a Configuration Application.
This approach to configuration management is popular because it centralizes the configuration at the master station (Geo SCADA Expert). It also avoids the potential problem of conflicting changes being made locally in the Field Device and in Geo SCADA Expert.
 - 
                    
Use the vendor-supplied configuration tool to make the changes locally, and then upload the changes into Geo SCADA Expert. Local configuration is used when the engineers on site do not have remote access to Geo SCADA Expert. Instead, they configure the Field Device locally.
 - 
                    
Use the Field Device's Configuration Application to make changes to the bulk configuration and then load the modified configuration into the Field Device. You will also need to import the modified bulk configuration file into Geo SCADA Expert. This avoids the need to upload or download configuration, and so can be used when upload/download is not supported or if communications are too slow or unreliable.
 
For more details, see Using a Configuration Application to Change Field Device Configuration
If the configuration of a Field Device is changed locally, you can choose to overwrite the Geo SCADA Expert configuration with the local configuration. Alternatively, you can overwrite the local configuration with the Geo SCADA Expert configuration, or you can accept that the configuration is different (see Accept Local Configuration).
Further Information
For information on the various ways of configuring a WITS Field Device to interoperate with Geo SCADA Expert for the first time, see WITS Configuration Strategies.