Configure the Connection for the Geo SCADA Expert Client

The first step when setting up a third-party ODBC client connection is to configure the connection for the Geo SCADA Expert client:

  1. Log on to Windows on the PC that is running the third-party application(s).
  2. Run the Geo SCADA Expert Client applet (see Display the Geo SCADA Expert Client Applet).
  3. At the User Account Control prompt, select Continue to allow the Geo SCADA Expert Client applet to run.
  4. When the Geo SCADA Expert Client applet runs, select the Add button to display the Geo SCADA Expert Client Configuration window.
  5. Use the Geo SCADA Expert Client Configuration window to create a new connection. The configuration you need to define is exactly the same as that for a ViewX - System connection, with these settings available:
  6. When you have defined the connection settings, select the OK button to apply them.
    The Client Configuration window is closed and the new connection is added to the list on the Geo SCADA Expert Client applet.
  7. Select the Licenses button to display the Client Licensing window. Use this window to associate the third-party ODBC client with a data access license (see Associate a Third-Party ODBC Client - System with a Data Access License).
  8. Close the Geo SCADA Expert Client applet.

Next, you need to access the ODBC Data Source Administrator Tool.

Further Information

64-Bit Applications Running on Windows.


Disclaimer

Geo SCADA Expert 2021