Failed Client - System and Server Advise Connections

If the client - system connection or the server advise connection cannot be established, ViewX will show the system as being 'Offline'. Users will not be able to use the client to interact with your system.

The connections will fail to establish if:

Further Information

Firewall Settings for Client - System and Server Advise Connections.

Understanding Client - System and Server Advise Connections.

Certificates for Geo SCADA Expert Server and Client Connections.

Use the Server Status Tool to ascertain the current status of server - client connections: see Server Status Information.

Enable or Disable IPv6 on the Client.


Disclaimer

Geo SCADA Expert 2021