Move an Event

This section applies to Schedules other than Simple Schedules.

To move an event to a new location on the same tab on a Schedule Display:

  1. Display the Schedule in Design Mode.
  2. Select the event that you want to move—do not release the mouse button.

  3. Drag the event to its new location. The event marker changes color, as the event marker is moved the original position is also shown.

  4. Release the mouse button at the required point.
  5. Repeat steps 2 to 4 for any other events that you need to move.
  6. Save the configuration (see Saving Configuration Changes).

To move an event from one tab to another on a Schedule Display (for instance, from one day to another, or from one month to another):

  1. Delete the event from the tab on which it is no longer required (see Delete an Event).
  2. Select the tab on which you want to insert the event.
  3. Add the event at the required time and date (see Add an Event Directly to a Schedule).
  4. Repeat steps 1 to 3 for any other events that need moving to other tabs.
  5. Save the configuration (see Saving Configuration Changes).

To move an event by using the Schedule Times window:

  1. Display the Schedule Times Window.
  2. Select the event that you want to move.
  3. Select the Edit button.
    The Edit Time window is displayed, with the first element of the time or date highlighted.

  4. To change a day, month, or Calendar day type, use the Up and Down arrow keys on your keyboard to cycle through the available options and select the required entry.
  5. To change a time element (for instance the hour), select that element and then either overwrite the time, or use the field’s arrows to select the required time.
  6. Select the OK button to update the entry in the Schedule Times window.
  7. Repeat steps 2 to 6 for any other times that you want to edit in the window.
  8. Select the OK button on the Schedule Times window to update the event times in the Schedule Display.
  9. Save the configuration.

Disclaimer

Geo SCADA Expert 2021