Using Parameters to Store Static Data Values

Geo SCADA Expert supports a series of Parameters that can be used to store static data values, such as a postal address, or map grid reference. Consider using Parameters if the data that you want Geo SCADA Expert to store is:

You can use Parameters, for example:

Unlike Variables or Internal Points, users need the Configure permission, rather than the Control permission, to change a Parameter’s value. This provides additional security to help ensure that data that is intended to remain static is only changed by users with that permission.

This section:

It also explains how to:

Also included is a series of examples that demonstrate how Parameters might be used on a Geo SCADA Expert system (see Example Configuration).


Disclaimer

Geo SCADA Expert 2021