Define whether the Alarm Limits can be Tuned

The Tune Limits field is displayed toward the bottom of the Alarm Limits section on the Analog Point tab:

Any alarm limits to which tuning is applied will remain tuned when the Tune Limits check box is clear. Use the Tune Alarm Limits pick action to remove the applied tuning.


Disclaimer

Geo SCADA Expert 2021