Pulse actions on several drivers support a combination of these status attributes:
- Id
- Full Name
- Type
- Position
- Created—(New pulse actions only)
- Last Modified
- Configuration Change CRC—(Only displayed if this feature is enabled on your system)
- Exclusive Control User—(Only pulse actions that are under Exclusive Control)
- Queued Request—(Pulse actions for which pick action requests are queued)
- Alarm State
- Alarm Last Updated
- Control Alarm
- Alarm Count
- Suppression Status—(Pulse actions on which Alarm Suppression is configured)
- Suppressing Parent—(Pulse actions on which alarms are currently suppressed)
- Source Name
- Source
- Current Quality
- Control Active—(Pulse actions on advanced drivers only)
- Last Control—(Pulse actions on advanced drivers only)
- Last Pulse Action—(Pulse actions on advanced drivers only)
- Controls
- Control Feedback Point—(only displayed if control feedback is enabled and there is a feedback check point associated with the pulse action)
- Waiting For Feedback—(only displayed if control feedback is enabled and there is a feedback check point associated with the pulse action)
- Last Feedback Timed Out(only displayed if control feedback is enabled and there is a feedback check point associated with the pulse action)
- Uncommanded Change Point(only displayed if uncommanded change detection is enabled and there is an uncommanded change check point associated with the pulse action)
- Has Uncommanded Change(only displayed if uncommanded change detection is enabled and there is an uncommanded change check point associated with the pulse action).
For information on pulse action status attributes that are not listed above, see the driver-specific documentation.