Specify the Control Value Maps

Use the fields within the Control Value Maps section of the Value Maps tab to specify the Filtered Value Maps that store the output data for this slave outstation. The Filtered Value Maps that store a slave outstation’s data have to exist on your system before you can use the fields below to map to such data. (For more information, see Specify the Filtered Value Maps that Store the Source Data, and see Configuring Value Maps in the Geo SCADA Expert Guide to Core Configuration.)

Leave the fields blank for any Control Value Map types that are not used by this slave outstation.

The Control Value Maps section also includes fields that you use to specify the:


Disclaimer

Geo SCADA Expert 2021