Work with Common List Options

Geo SCADA Expert provides you with a set of common List options that allow you to change how the information on a List is displayed. When you display a List, you can right-click on an entry in order to display a context-sensitive menu. You then select the menu option that you require:

With Lists that are embedded on Mimics you select (rather than double-click) on an entry in the List to display that entry's context-sensitive menu.

Further Information

Display a Historic List.

Display a Queries List.

Events Lists.

Understand Historic Lists.


Disclaimer

Geo SCADA Expert 2021