Configure the Server and Publishing Properties

The Subscription tab of the OPC UA Subscription Form includes the following properties:

When Geo SCADA Expert requests that an OPC UA server starts to monitor an item, that OPC UA server will respond with the actual values that it is using for such monitoring. This includes values for some of the properties that you can configure on the configuration Form of the OPC UA Subscription or OPC UA Point. The 'Actual...' series of status attributes indicate the values that the OPC UA server is actually using, which might well be the same values as those configured on the configuration Form of the OPC UA Subscription or OPC UA Point.

For more information about the 'Actual...' series of status attributes on an OPC UA Subscription, see Status Attributes that are Specific to OPC UA Subscription Items.


Disclaimer

Geo SCADA Expert 2021