Configuring SCADAPack Modbus Realflo Controllers

Geo SCADA Expert has the ability to monitor flow calculation data from a Realflo-enabled SCADAPack controller (a SCADAPack controller that is a gas flow computer). For each SCADAPack controller that is running Realflo and for which you want Geo SCADA Expert to process flow data, you need to add and configure a suitable SCADAPack Modbus Realflo controller in the Geo SCADA Expert database.

The SCADAPack Modbus Realflo driver supports these types of Realflo controller (outstation):

If your database structure is ‘modular’ and Group Templates are used to store ‘model’ SCADAPack Modbus Realflo configuration, in addition to the above types of controller, you can add this driver-specific ‘abstract’ controller item to your Group Templates:

You can only add Abstract Items to Group Templates. The abstract items appear as additional driver-specific entries when you display the context sensitive menu from a Group Template. As with other abstract items, in order to represent a ‘real’ controller, you need to convert the abstract items into the required type of controller (outstation) within the Group Instances that reference the Group Template. For more information, see Add an Abstract Item to a Group Template in the Geo SCADA Expert Guide to Core Configuration.

 

You specify each controller’s properties using the fields on the appropriate Realflo Outstation Form. Each Realflo Outstation Form has several tabs.

Use the SCADAPack tab to:

Use the Realflo tab to:

Once you have configured a Realflo controller in Geo SCADA Expert, you need to create and configure the necessary Flow Run(s), and associate those Flow Run(s) with the Realflo controller (see Configuring a SCADAPack Modbus Flow Run).

The fields on other tabs are common to controllers and outstations on many advanced drivers (see Tabs on Outstation Forms in the Geo SCADA Expert Guide to Advanced Drivers).

For information on the minimal amount of configuration that you can undertake to produce a functional Realflo-enabled SCADAPack controller in Geo SCADA Expert, see Minimum Configuration.


Disclaimer

Geo SCADA Expert 2021