Liquid Flow Run Properties

For a Liquid Flow Run use the fields on the Liquid tab of the Flow Run Form to Configure the Flow Run Properties.

You can configure these properties directly in Geo SCADA Expert, or read the configuration into the Geo SCADA Expert database (see Configure or Read the Flow Run Configuration).

With the properties listed below, you can either Configure or Read the Flow Run Configuration.


Disclaimer

Geo SCADA Expert 2021