Set up a Port Server

Geo SCADA Expert includes an application called a 'port server' that can provide:

To setup a port server:

  1. Determine which type of Port Server Setup provides the functionality you require.
  2. Install the Port Server Software.
  3. Configure a Static Serial Port if required (this is dependent on the type of port server setup).
  4. Restart the Port Server Service.
  5. Create the Channels in the Database.

For assistance with common issues relating to port server setup, please refer to one of the following sections:

To determine which one of these sections is applicable to your setup, you should first learn about the different port server setups (see Port Server Setup).


Disclaimer

Geo SCADA Expert 2021