Disable Database Emulation after a Successful Upgrade

Do not disable Database Emulation if you intend downgrading the version of Geo SCADA Expert software that is currently running on the servers on your system. Instead, if Database Emulation was enabled for the upgrade and has remained enabled since then, leave that Database Emulation enabled while you perform the downgrade (see Perform a Downgrade after Upgrading Geo SCADA Expert).

If you enabled Database Emulation when you upgraded the version of Geo SCADA Expert software that was running on your servers, once you have confirmed that the upgrade is successful on your system, you should disable that Database Emulation. You have to do this on each Geo SCADA Expert server on which Database Emulation is enabled. This will cause each server to stop. Therefore in a multi-server architecture, you might want to disable Database Emulation on each of the standby servers first, before you shut down and then disable it on the Main server. This will result in a single Changeover (rather than multiple changeovers if you disabled Database Emulation on the Main server first, or partway through disabling the feature on each of your servers). For detailed steps on how to do this, select the relevant link below:

To disable Database Emulation:

  1. Ensure that all of your servers have been upgraded to run the same build of Geo SCADA Expert software.

  2. See above for the suggested order in which you should disable this feature on the servers on your system.

  3. Right-click on the Server icon in the taskbar in Windows.
    A context-sensitive menu is displayed.

  4. Select the Deactivate database version emulation option. (This option is only available when Database Emulation is enabled on the server.)
    On a multi-server system, the server will shut down. On a lone server system, the server will remain running. Database Emulation will be disabled on the server.

  5. With a lone server system, you can ignore the rest of the steps in this procedure.

    With a multi-server system, restart the server.

  6. With a multi-server system, repeat the above steps on the other Geo SCADA Expert servers on which Database Emulation is enabled.

    (On a triple redundant system (see Triple Standby Architecture), this will enable that system to retain at least dual redundancy throughout this phase of the upgrade process.)

Once Database Emulation has been disabled:

When you upgrade the version of Geo SCADA Expert software that is running on a server, the setting that was specified for Database Emulation in the Installation Wizard gets stored on that server (see Database Emulation Configuration). This same setting is then offered by default when the server is next upgraded. Deactivation of Database Emulation via the Server Icon only disables that feature on the version of upgraded Geo SCADA Expert software that is currently running on the server; it does not affect the setting used for Database Emulation in the Installation Wizard. (To change the setting that is offered by default when the server is next upgraded, you use the Server Configuration Tool (see Specify the Default Setting for the Database Emulation Feature).)


Disclaimer

Geo SCADA Expert 2021