Display an X-Y-Z Plot in Run Mode

Operator-level users (users that operate the system, rather than configure it) need to use X-Y-Z Plots in Run mode. When an X-Y-Z Plot is displayed in Run mode, users can access navigation features and use them to view and compare data on the Plot.

On a ViewX client, security permissions and menu options determine whether you display X-Y-Z Plots in Run mode or Design mode.

On a Virtual ViewX client or an Original WebX client, you can only display X-Y-Z Plots in Run mode.

To display an X-Y-Z Plot in Run mode on a ViewX client or Virtual ViewX client:

  1. Log on to ViewX or Virtual ViewX via a User Account that has the Operate feature enabled (on the User Form) and has the Read and Browse permissions for the X-Y-Z Plot (or its parent Group).
  2. Display the Database Bar (see Display an Explorer Bar).
  3. In the Database Bar, locate the X-Y-Z Plot that you want to display in Run mode.
  4. Right-click on the X-Y-Z Plot in the Database Bar.
    A context-sensitive menu is displayed.
  5. Select the Display X-Y-Z Plot pick action.
    The X-Y-Z Plot is displayed in Run mode.

Alternatively, you can display an X-Y-Z Plot in Run mode by performing one of the following:

Or:

Or:

  1. Right-click on the X-Y-Z Plot in a Queries List.
  2. Select the Display option.

Or:

Or:

  1. Display the X-Y-Z Plot in Design mode (see Display an X-Y-Z Plot in Design Mode).
  2. Perform one of the following:
    • Deselect the Design Mode button on the Quick Access Toolbar.

      Or:

    • Deselect the Design Mode command on the ViewX ribbon's Edit tab.

On an Original WebX client, you display and operate X-Y-Z Plots in a similar way to pre-configured Trends (see View and Action Trends on an Original WebX Client).


Disclaimer

Geo SCADA Expert 2021