ViewX Client - Third Party OPC Server Connections
As Geo SCADA Expert supports OPC standards, a ViewX client can be configured to connect to a Third Party OPC server, such as a Kepware OPC server or a Matrikon OPC server. This means that a ViewX client can be used to connect to Geo SCADA Expert and many other OPC based systems—providing that there is a suitable connection for each server.
In this section, we explain how to: