The Effects of Suppression on Alarm Displays
The tables in this topic explain the effects that 'By Alarm State' and 'By Expression' alarm suppression have on the entries in alarm displays.

The table below indicates how the alarm condition that triggers 'By Alarm' alarm suppression affects the entries in alarm displays, such as Alarms Lists and the Alarm Banner.
The two columns on the left relate to activity on the 'parent' database item (the item that triggers the suppression). The columns on the right relate to alarm activity on each 'child' database item (the items on which alarms are to be suppressed).
Activity on Parent Database Item | Alarm Activity on Child Database Items | |||
---|---|---|---|---|
Parent Alarm Activity | Entry in Alarm Displays | Child Alarm Activity | Alarm Status | Entries in Alarm Displays |
No active alarms |
--- |
Any alarms |
Unacknowledged Uncleared/ |
VISIBLE |
Alarm that triggers alarm suppression raised |
VISIBLE |
The effect on the alarms of child database items on which the 'Suppress Pre-existing Alarms' property is disabled: |
||
Existing alarms that were raised pre-suppression |
Unacknowledged Uncleared/ Acknowledged Uncleared |
VISIBLE |
||
Alarms that cleared pre-suppression, which remain unacknowledged (Geo SCADA Expert automatically acknowledges any alarms that have already cleared when suppression comes into force) |
---
|
--- |
||
Existing alarms, raised pre-suppression, which have been acknowledged while suppression is in force |
Acknowledged Uncleared |
VISIBLE |
||
Alarms raised while suppression is in force |
Unacknowledged Uncleared |
Suppressed (not shown) |
||
Alarms raised while suppression is in force and which have cleared while suppressed (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed) |
--- |
--- |
||
Alarm that triggers alarm suppression raised | VISIBLE | The effect on the alarms of child database items on which the 'Suppress Pre-existing Alarms' property is enabled: | ||
Existing alarms that were raised pre-suppression | Unacknowledged Uncleared |
Suppressed (not shown) |
||
Acknowledged Uncleared |
VISIBLE (This is by design, as an acknowledged alarm indicates that operators have been investigating the cause and might want to check that the abnormal condition that caused the alarm does clear.) |
|||
Alarms that cleared pre-suppression, which remain unacknowledged (Geo SCADA Expert automatically acknowledges any alarms that have already cleared when suppression comes into force) | --- |
--- |
||
Alarms raised while suppression is in force | Unacknowledged Uncleared |
Suppressed (not shown) |
||
Alarms raised while suppression is in force and which clear while suppressed (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed) | --- | --- | ||
Alarm that triggers alarm suppression cleared, 'Unsuppress Delay' in force |
VISIBLE (Unacknowledged Cleared)/ |
Alarms raised while the 'Unsuppress Delay' is in force and which clear while that delay remains in force (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed) |
--- |
---- |
Any remaining alarms that were raised either during the suppression or during any 'Unsuppress Delay' that occurred following that suppression. |
Unacknowledged Uncleared/ Acknowledged Uncleared |
Suppressed (not shown) | ||
Alarm that triggers alarm suppression cleared, 'Unsuppress Delay' expired | VISIBLE (Unacknowledged Cleared)/ --- (once acknowledged) |
Any alarms, regardless of whether they were raised pre-, post-, or during suppression, or during any 'Unsuppress Delay' that occurred following that suppression. |
Unacknowledged Uncleared/ Acknowledged Uncleared | VISIBLE* |
Different type of alarm raised** |
VISIBLE |
Any alarms, regardless of whether they were raised before or while the parent object’s alarm is active |
Unacknowledged Uncleared/ Acknowledged Uncleared/ Unacknowledged Cleared |
VISIBLE |

The table below indicates how the expression criteria that triggers 'By Expression' alarm suppression affects the entries in alarm displays, such as Alarms Lists and the Alarm Banner.
The column on the left relates to activity on the 'parent' database item (the item that triggers the suppression). The columns on the right relate to alarm activity on each 'child' database item (the items on which alarms are to be suppressed).
Value of the Parent Alarm Tag | Alarm Activity on Child Database Items | ||
---|---|---|---|
Child Objects | Alarm Status | Entries in Alarm Displays | |
Causes the expression to evaluate as 'False' (no suppression) |
Any alarms |
Unacknowledged Uncleared/ |
VISIBLE |
Fulfills the expression criteria |
The effect on the alarms of child database items on which the 'Suppress Pre-existing Alarms' property is disabled: |
||
Existing alarms that were raised pre-suppression |
Unacknowledged Uncleared/ Acknowledged Uncleared |
VISIBLE |
|
Alarms that cleared pre-suppression, which remain unacknowledged (Geo SCADA Expert automatically acknowledges any alarms that have already cleared when suppression comes into force) |
---
|
--- |
|
Existing alarms, raised pre-suppression, which have been acknowledged while suppression is in force |
Acknowledged Uncleared |
VISIBLE |
|
Alarms raised while suppression is in force |
Unacknowledged Uncleared |
Suppressed (not shown) |
|
Alarms raised while suppression is in force and which have cleared while suppressed (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed) |
--- |
--- |
|
Fulfills the expression criteria | The effect on the alarms of child database items on which the 'Suppress Pre-existing Alarms' property is enabled: | ||
Existing alarms that were raised pre-suppression | Unacknowledged Uncleared |
Suppressed (not shown) |
|
Acknowledged Uncleared |
VISIBLE (This is by design, as an acknowledged alarm indicates that operators have been investigating the cause and might want to check that the abnormal condition that caused the alarm does clear.) |
||
Alarms that cleared pre-suppression, which remain unacknowledged (Geo SCADA Expert automatically acknowledges any alarms that have already cleared when suppression comes into force) | --- |
--- |
|
Alarms raised while suppression is in force | Unacknowledged Uncleared |
Suppressed (not shown) |
|
Alarms raised while suppression is in force and which clear while suppressed (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed) | --- | --- | |
Changes to a value that causes the suppression to clear, 'Unsuppress Delay' in force |
Alarms raised while the 'Unsuppress Delay' is in force and which clear while that delay remains in force (Geo SCADA Expert automatically acknowledges any alarms that are raised then clear while still suppressed) |
--- |
---- |
Any remaining alarms that were raised either during the suppression or during any 'Unsuppress Delay' that occurred following that suppression. |
Unacknowledged Uncleared/ Acknowledged Uncleared |
Suppressed (not shown) | |
Has a value that causes the suppression to clear, 'Unsuppress Delay' expired |
Any alarms, regardless of whether they were raised pre-, post-, or during suppression, or during any 'Unsuppress Delay' that occurred following that suppression. |
Unacknowledged Uncleared/ Acknowledged Uncleared | VISIBLE* |
* The date and time assigned to any alarms that were suppressed but become visible once suppression is no longer in force varies, depending whether the Use Visible Time As Alarm Active Time feature is enabled. If the feature is enabled, the alarm entries are time stamped with the date and time that they became visible post-suppression; if the feature is disabled (the default on most systems), the alarm entries retain their original time stamp (indicating the alarm’s original receipt time or occurrence time).
** Only some types of database item support more than one type of alarm.
Further Information
Activities that Occur when an Alarm is Raised.
Define whether the Visible Time is used as the Active Alarm Time.
For more information about either type of alarm suppression, see Configure any Alarm Suppression Requirements.