Point Updates to which Compression Settings do not Apply

If you Apply Historic Data Compression Settings to a point, Geo SCADA Expert compares the update that it last stored historically for the point and the next update that is marked for compression. If any of the following point attributes differ between the two values, Geo SCADA Expert ignores any Compression settings and automatically stores the latest update historically:

Additionally, Geo SCADA Expert also stores any ‘out of sequence’ data historically. Out of sequence data comprises values that are time stamped with an earlier time to the previously stored value.

You can determine why Geo SCADA Expert has stored an update historically, by looking at the Historic List for the point. Each of the above attributes are displayed in separate columns on the List.

If Master Station Alarm Limits are enabled and used for the analog points on your system, the ‘State’ column on the Historic List displays the Master Station State, rather than the ‘standard’ point State.

For further information on Historic Lists, see Historic Lists in the Geo SCADA Expert Guide to Lists.


Disclaimer

Geo SCADA Expert 2022