Supported File Types

The types of file that you can download to a SCADAPack E outstation via Geo SCADA Expert include:

In order to import any of these files successfully into Geo SCADA Expert, you need to ensure that the files comply with certain File Restrictions.

Whenever Geo SCADA Expert downloads any RTU Configuration files to a DNP3 SCADAPack E outstation, a log file is added to the list in the Configuration Setup window. You can use this ASCII file for diagnostic purposes (see Configuration Log File).


Disclaimer

Geo SCADA Expert 2022