Configure MQTT JSON Schema A Digital Points

With the MQTT JSON Schema A driver, you use:

You configure the properties of each digital point using fields on the MQTT JSON Schema A Digital Point Form. The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

The Digital Point tab includes properties that are specific to MQTT JSON Schema A Digital Points.

Use the Digital Point tab to:

Further Information

Minimum Configuration.


Disclaimer

Geo SCADA Expert 2022