Use a Mimic to Display another Mimic

Mimics can be configured so that they contain:

If you display a Mimic that contains a hyperlink to another Mimic or provides access to a Mimic’s context sensitive menu, you can use that Mimic to display other Mimics:

Either:

Or:

Or:

When you use a Mimic to display another Mimic, the ‘target’ Mimic (the Mimic that is displayed when you select the hyperlink or action) can be shown in place of the original Mimic, in a new window, or in an inset window. You can use the navigation features of ViewX or the web browser used by Virtual ViewX to move between the Mimics as required (see Use the Navigation Features to Display a Mimic).


Disclaimer

Geo SCADA Expert 2022