Use the Database Bar to Display a Mimic

You can use the Database Bar in ViewX to access Mimics and their various display options (see Display an Explorer Bar in ViewX in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients).

There are several ways of displaying a Mimic from the Database Bar:

With a ViewX client on a Multi-Monitor Setup, you may be able to select the name of the Window Container in which to display or edit a document. Each Window Container displays on a particular monitor by default. Such options are only available when you select certain Display... or Edit... pick actions from the Database Bar or Operator Documents Bar. For more information, see Ability to Specify the Window Container in which to Display or Edit a Document.

Further Information

Database Bar: see Explorer Bars in the Geo SCADA Expert Guide to ViewX and Virtual ViewX Clients.

The Mimic Display.


Disclaimer

Geo SCADA Expert 2022