OPC UA Specific Alarm and Event Categories
Each
You can optionally filter the entries in
On systems on which this driver is installed, in addition to the ‘core’ alarm and event categories, these driver-specific categories are available:
- OPC UA Point—Entries that are associated with OPC UA point activity.
- OPC UA Point Server State—Entries that indicate the state of an OPC UA Point in the database. For example, to show that a Point database item was not successfully added to an OPC UA Subscription.
- OPC UA Server—Entries that indicate the state of an OPC UA Server.
- OPC UA Subscription State—Entries that indicate the state of an OPC UA Subscription.