Points Used on OPC UA Servers

With the OPC UA driver, you create and configure one OPC UA Point per item of data that you want to monitor and/or control on an OPC UA server.

You have to configure points of the appropriate type to represent the type of data that you want the driver to retrieve and process.

The driver supports the following types of point:

You configure each point using the appropriate OPC UA Point Form. The configuration Form contains many fields, organized into tabs. Most of these tabs contain properties that are common to points on many drivers (see Tabs on Point Forms in the Geo SCADA Expert Guide to Advanced Drivers).

Properties on the <Point Type> tab comprise:

Further Information

Create a Point and Display a Point Form: see Create and Configure a Point in the Geo SCADA Expert Guide to Core Point Configuration.


Disclaimer

Geo SCADA Expert 2022