SCADAPack x70

Alarm Limits

Associated with: SCADAPack x70 analog and counter Configuration items, protocol-specific analog points and counter points on which alarm limits are currently tuned and/or the Multiple Alarm Limits feature is enabled.

In the SCADAPack x70 driver, the multiple alarm limits are inherited from the group containing the associated Configuration item rather than the group containing the protocol-specific point.

This status attribute is only displayed for points and Configuration items on which:

The attribute lists the following:

If multiple alarm limits are enabled and the alarm limits are also tuned, tuning takes precedence over multiple alarm limits.


Disclaimer

Geo SCADA Expert 2022